Blog > Automation > Avoid Ground Loops with Signal Conditioners
12/11/19 | Tom Hopkins, Rexel Technical Consultant
Erroneous input data in your industrial process can cause problems. Ground loop noise can adversely impact process data (temperature, pressure, flow, etc.). Because this data can be critical to an industrial process, it’s important to understand the possibility of this noise, what causes it, and how to remediate the issue.
If two devices are connected, yet grounded in different locations, there can be a difference in potential between those two grounds. As you may know, a difference in potential in a circuit is going to induce a flow of electrons. This will create a loop current that is known as a “ground loop.” Since the induced current runs along the same wires as the analog signal, the noise of the ground loop will often cause erroneous signal data.

If you put a break in the ground loop circuit, the induced current will stop, and your signal will be undisturbed. Breaking the circuit is called “isolation.” But how will your signal get through if you break the electrical connection? This is done by adding a specialized device that is called a signal conditioner or an optical isolator. The signal conditioner still allows the passing of your signal without an electrical connection.

© Rockwell Automation
How a Signal Conditioner Works
A signal conditioner works by taking the input signal and converting it into optical signals with an LED. That LED then sends light to a photodiode that converts the signal back to electrical. You can see why another name for this device is an “optical isolator.” Through the simple brilliance of this device, the signal can pass through without an electrical connection, and the ground loop problem is averted.
Using the same isolation technology enables you to do other helpful things.

Now that you understand signal conditioners, you may be thinking: “This is great stuff! Where do I find these magic devices to help me with my industrial process?” Rockwell Automation has a comprehensive line up of signal conditioners. You can learn more here. And if you have questions or are ready to get started with this technology, contact us today.